Other Parts Discussed in Thread: ADS1256,
Hello,
I would like to measure conversion time and compare it with the t18. The SPI master sends:
- SYNC command
- Wait t11
- WAKEUP command
fCLKIN = 7.68MHz.
The settling time is measured starting at the WAKEUP is sent event and ends when DRDY/ goes low. Unfortunately, measurement via DRDY/ low-high-low is not possible because sometimes the SYNC and WAKEUP are sent during already running conversion and DRDY/ does not go low.
According to the datasheet the "synchronization occurs on the first rising edge of the master clock after the first SCLK used to shift in the WAKEUP command.". The term synchronization is not explained further in this case with respect to the DRDY/ line. For SYNC/PDWN/ line is clearly specified when the DRDY/ goes low or high and when the conversion is started. This information is missing for the SYNC command.
What I have observed, there is always a delay of ~2.5 us between first SPI clock of the WAKEUP command and DRDY/ low-high transition. This number was measured together with several SPI speeds. However I could not find any datasheet value which would be close to it.
Can be the total conversion time considered as t18 + 2.5us?
Best regards
Martin Velek