Good day Colleagues,
Could you help to undestand output data rate question from my customer? he is using the ADS131E08.
Internal clock is 2.048MHz. Customer tried to set different DR CONFIG1 settings, but always got data rate and /DRDY signal two times lower than it should be.
For example, he used value of 101 and instead of 2kHz he got 1kHz.
he also checked register's values and they were setup correctly. he also tried to use differenct SPI clock (6, 10, 20MHz) but DRDY signal every time is two limes lower value.
Could you tell me what he should check? Or what can be wrong in here?
Thank you, Mikhail