Part Number: ADS1298
Other Parts Discussed in Thread: ADS1299
Hello
I need connect 4 ADS1298 to build a 32 channel system. But I have some problems. I wish you could help me with this questions.
1-Is it better to use bipolar or single supply? What are advantages and disadvantages of every method? In which applications, it's better to use single supply?
2-In page 58 of datasheet it said it's better to minimizing length of DOUT to minimize board-level signal delays . but in next sentences it said Placing delay circuits such as buffers between DOUT and DAISY_IN is another way to mitigate this challenge. One other option is to insert a D flip-flop between DOUT and DAISY_IN clocked on an inverted SCLK.
3-Is there any other PCB consideration about Daisy connected ADS129Xs?(Except points on page 58 of datasheet)
4- I want to get data from 32 differential channels (64 channels) on 4mm*4mm array electrode. For this small electrodes and small distance between individual electrode,Is it necessary to use GND electrode (RLD pins in ADS1298 and BIAS pins in ADS1299) to reduce common mode noise?
thanks very very much :)