This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8168EVM-PDK: ADS8168

Part Number: ADS8168EVM-PDK
Other Parts Discussed in Thread: ADS8168

Hello.

I am testing the ADC platform/board to capture samples. However, the capture size is too small using the supplied GUI.

Is it possible to get the API that is used to collect the data from the hardware so I can develop my own user interface?

Thanks,

Malcolm

  • Hello Malcolm, The GUI source code is not available for the ADS8168 evaluation board. Modified code will not increase sample size because the maximum sample size is limited in hardware to the available memory. You can remove the data capture card (PHI board) and connect your own MCU/data capture hardware if more than 2 million samples are needed. Regards, Keith Nicholas Precision ADC Applications