Hello,
I see in the DAC80508 datasheet that the SCLK speed is limited during SPI read transactions. Those frequencies are details in Table 7 of the datasheet.
Is the limitation of the read speed due to the SDO output drive strength? For example, assuming FSDO = 0, VIO = 3.3V, and given the figure below; would we be able to use SCLK = 50MHz for frame #1, and then SCLK = 18MHz for frame #2?
Don