This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC80508: RTE thermal pad

Part Number: DAC80508

In the datasheet for the part, there are two images of the exposed thermal pad.

4205254

4206446

Which one is correct for DAC80508ZRTET?

  • Hi Greg,

    The second diagram is correct.  Note that the first one has a generic/placeholder thermal pad, but it does not provide any dimensions for it it.  The second image has the exact dimensions for this device.  The RTE package is used on multiple devices, but the thermal pad is usually die specific.  

    Thanks,

    Paul