Dear Team,
My customer is evaluating the ADS1120-Q1 with K-Type Thermocouple in their system. However, there is a slight difference in temperature between the actual thermocouple contact and the temperature sensor value inside the ADS1120-Q1, and the temperature of the measurement is displayed as an error.
In order to perform the temperature simulation, could you give us information on the structure of the ADS1120-Q1 or the thermal resistance from the terminal (AIN#) to the internal temperature sensor?
To eliminate this temperature difference, their goal is to extract parameters such as pattern, via placement, board thickness, and so on by thermal simulation.
They want information as a parameter that allows heat transmitted through the board to reach the internal temperature sensor, not the self-heat generated by the component.
I look forward to your reply.
Thank you.
Best Regards,
Koshi Ninomiya