Hi,
My customer wants to use ADS7828E/250G4. However, I didn't find ESD rating parameters from the datasheet, which are needed in customer company's AVL process.
Could you help to provide it?
Thanks,
Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer wants to use ADS7828E/250G4. However, I didn't find ESD rating parameters from the datasheet, which are needed in customer company's AVL process.
Could you help to provide it?
Thanks,
Andrew
Hello,
Here are the ESD ratings of the devices:
HBM | CDM | MM | |
ADS7828E/250 | 2kV | 1kV | 250V |
ADS7828E/2K5 | 2kV | 1kV | 250V |