Part Number: DAC7822
Other Parts Discussed in Thread: OPA2822
Dear all,
I have the following design (see picture attached) using DAC7822.
I need a voltage output of the DAC in the range 0 to +1,2V, so according to the datasheet of DAC7822, the VREF should be -1,2V.
This negative reference is generated using a ADR3412 and a OPA2822. What I see in TP38 is a oscillation as shown in the picture. This oscillation stay even when I am not powering the DAC (3V3D off), that is, stay when all the digital electronic of the board is off.

In the the picture below, the +5V_DAC signal is shown.

Any advise to improve this? What could be the cause? Could be the DAC causing this?
Any comment will be welcome.
Maybe this is not the forum to place this, in that case, please, let me know, and I will forward to the right place.
Thanks in advance,
Joaquin.