I want to know ADS1256 can work in Differential Inputs with 1 -2 3-4 5-6 and Single-Ended with 7 8. If it can work I think the AINCOM should tied to a midpoint reference .Is that so?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to know ADS1256 can work in Differential Inputs with 1 -2 3-4 5-6 and Single-Ended with 7 8. If it can work I think the AINCOM should tied to a midpoint reference .Is that so?
Hi Xiaoqing,
You can see in the ADS1256's MUX register that you can select any analog input as AINP or AINN. Therefore, the configuration you proposed is certainly valid, you would just need to change the value of the MUX register each time you want to change channels.
AINCOM could be tied to ground or to some other voltage, it really depends on the signals you are measuring and how you want to use the ADC's full-scale range. You should also consider that if the buffer is enabled then the input range is slightly limited and you should not be measuring ground-referenced signals with the buffer enabled.
-Bryan
Thank you for your reply,My Single-Ended signals is 0-VREFP and VREFN tied to ground,So AINCOM could be tied to ground.But datasheet say The following。

Hi Xiaoqing,
Yes, as I mentioned in my previous post, you can tie AINCOM to ground or you can tie AINCOM to some other voltage. The datasheet is just stating that AINCOM does not have to be tied to ground, as some designers might infer.
If you are measuring between 0 and VREFP, then you would want to tie AINCOM to VREFP/2 to be able to use the ADC's full code range.
-Bryan