Hi, am working with a customer on this device. They are operating with a FCLCK of 5MHz (and CLKDIV=0). Unfortunately they have to derate to 80% to meet their spec, so the Max 5.4Mhz x 0.8 is 4.3MHz. They may have to change to the CLKDIV=1, which has a Max FCLK of 27MHz. What happens when they still continue to run at 5Mhz operation with CLKDIV=1? Does the internal timing etc look the same between CLKDIV 0 and 1 since the operating frequency remains at 5MHz?
Thanks in advance.