Hello, Would you please lt me know about Q1 & Q2 about AIC3101 dual rate?
I can not find any description is the D/S.
QUESTIONs
( please refer to AIC3101 data sheet page 28 and page 30)
Q1 AIC3101 Dual rate enable/desable is NOT available when using CLKDIV?( We think so)
Q2 CODEC_CLK must be 256 x fs ? ( We think so)
BackGround
My customer use AIC3101 for audio recording and mass production should be soon.
Customer want to use AIC3101 under WCLK= 96KHz. ( hope freq responce 20Hz~ 40KHz) .
Other conditoin is following
/slave mode
/ use CLKDIV
/BCLK=64Fs =6.144MHz ( applied from external)
/Q=2
-------------------------------
"" Case 1 MCLK=128Fs=12.288MHz ""
・CLKDIV Q=2
・WCLK=1Fs=96kHz、BCLK=64Fs=6.144MHz Slave
・DUAL RATE MODE enable
==>>> No output found
Regardless of ADC/DACのPOWER Up/Down setting
"" Case 2 MCLK=256Fs=24.576MHz""
DUAL RATE MODE enable
Other setting is same as case1
==>>> works fine. freq responce 20Hz~40KHz almost flat.
"" Case 3 using PLL ""
・MCLK=128Fs=12.288MHz
・K=1.0 R=8 P=1
・WCLK=1Fs=96kHz、BCLK=64Fs=6.144MHz
・DUAL RATE MODE enable
==>>> works fine. freq responce 20Hz~40KHz almost flat.