Hello,
for my application I working with the pcm2906c which works fine on the WindowsXP , but on the Windows seven the input Line is recognized as a microphone input and the gain is very high. I can't find a setting in windows.
thanks,
Simon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Simon,
Can you confirm the part is PCM2906C and not PCM2906B? PCM2906C should be recognized as a line connector. This issue has been solved on C devices, an app note is linked here. (http://www.ti.com/lit/an/sbfa020/sbfa020.pdf)
Hi, Simon,
This device is going thru the final steps of our release process. It should be active next week.
-d2