This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3254EVM-U Hardware device not connected.

Hello,

In my company, we have 4 USB board TLV320AIC3254EVM-U.

2 are OK, and 2 do not work.

At the beginning, the  2 board were OK, the connection with PurePath Studio was OK, but after a few minutes (maybe a manipulation error in PurePath) the connection with the PC is lost, and I didn't manage to retrieve it.

On the 2 OK board, when I plug then on the PC, the LED is ON

On the 2 NOK board, the LED is OFF.

In purePath, the log is

"

Generating code for base_main_Rate44 .. assembling .....Done.

Build succeeded.
Hardware device not connected."


How can I  reset these board ?

Thanks for your help,