we taken tlv320aic31xx.c as the reference for the tlv320dac3100. Sound card is registered -- we are getting Audio routing problems and regulator and Remote IO error , below is the log:
tlv320aic31xx-codec 1-0018: ASoC: no sink widget found for HPLOUT
[ 2.606112] tlv320aic31xx-codec 1-0018: ASoC: Failed to add route Output Left -> Switch -> HPLOUT
[ 2.620089] tlv320aic31xx-codec 1-0018: ASoC: no sink widget found for HPROUT
[ 2.627722] tlv320aic31xx-codec 1-0018: ASoC: Failed to add route Output Right -> Switch -> HPROUT
[ 2.637300] evm_aic3x_init,np->name: sound : full name : /sound
[ 2.643646] evm_aic3x_init,ret:0
[ 2.647150] tlv320aic31xx-codec 1-0018: ASoC: DAPM unknown pin MONO_LOUT
[ 2.654261] tlv320aic31xx-codec 1-0018: ASoC: DAPM unknown pin HPLCOM
[ 2.661152] tlv320aic31xx-codec 1-0018: ASoC: DAPM unknown pin HPRCOM
[ 2.670229] davinci_evm sound.12: tlv320aic31xx-hifi <-> 4803c000.mcasp mapping ok
[ 2.680792] tlv320aic31xx-codec 1-0018: Failed to restore cache: -121
why this error is coming i am not getting : in the code it is related to regmap:
[ 2.885829] ALSA device list:
[ 2.889089] #0: AM335x-EVMSK
[ 4.549612] Error: Driver 'tlv320aic31xx-codec' is already registered, aborting...
[ 4.786730] Error: Driver 'davinci-mcasp' is already registered, aborting...
[ 5.614910] Error: Driver 'davinci_evm' is already registered, aborting...
ALSA: Restoring mixer settings...
No state is present for card AM335xEVMSK ----- this
Found hardware: "AM335x-EVMSK" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card AM335xEVMSK -- and this -- why two times this error was came --
As the card is loaded why this "NO State for card " error is occurring -- some thing we are missing -- in the setting or any configuration issue is there ???
--Please help in this --
in the dts file we given the audio routing as :
ti,audio-routing =
"Headphone Jack", "HPL",
"Headphone Jack", "HPR";
serializer :
serial-dir = < /* 0: INACTIVE, 1: TX, 2: RX */
0 0 1 2 -- we are using AXR2 as transmit and which is a DIN pin to the codec.
>;
one more error:
[ 2.680792] tlv320aic31xx-codec 1-0018: Failed to restore cache: -121
why this error is coming i am not getting : in the code it is related to regmap:
in the the codec drvier: tlv320aic31xx.c --code -- please let me know anything we are missing here ???
regcache_cache_only(aic31xx->regmap, false);
ret = regcache_sync(aic31xx->regmap);
if (ret != 0) {
dev_err(codec->dev,
"Failed to restore cache: %d\n", ret);
regcache_cache_only(aic31xx->regmap, true);
regulator_bulk_disable(ARRAY_SIZE(aic31xx->supplies),
aic31xx->supplies);
return ret;
}
Thanks in advance ... waiting for the reply from anyone..
regards,
Viswanath K.