Other Parts Discussed in Thread: PCM1794, LM317, PCM1794A
Hi for all,
I have an intresting phenomenon with this DAC IC-s. I guess what the problem can be, but would like to have a confirmation.
I have built a multichannel DAC with PCM1794. There are 4 separate (1 layer, through hole) panels with one IC pro panel in stereo mode with I2S inputs.
The receiver is the MiniDSP USBStreamer (I2S output). Please see attached picture (it is not my actual setup(!), only my first test arrangement with only one panel).
The problem comes when only rarely, as I turn on the system, or: I turn on-off only the PSU of the OPAs. In this case, the current consumption of the DAC on the 3,3V (digital) side is going to be the 5-10x of the normal, the IC is getting very warm, an there is no sound coming out...:( I turn of course immediately out, and next time everything normal....
So my suspect: the problem can be that the digital and analog grounds are not connected directly by the DAC IC, but also at the PSU (see short connection). I have made it so because I have 4 panels and only one (double) PSU, and I wanted to avoid ground loops!
Is my insight correct? How shoud I arrange this setup to have a good and stable layout?
Thanks!!
(more pictures or shematics are of course by request available!)