Hello,
I am using PurePath Studio to configure an AIC3204 eval module. I am able to use the graphical interface to adjust the sample rate up to 48kHz, but if I select rates >48kHz I start seeing junk output in all cases I can't find instructions anywhere in the user guide.
1) Can you please provide step-by-step instructions for how to configure the eval board to run at 96 kHz and at 192kHz?
2) Secondly, there is brief mention in the datasheet regarding the minidsp performance at 48kHz. Can the minidsp run at sample rates >48kHz, or is this a limit?
For reference, my setup involves passing an impulse from a function generator into the input of the board, and displaying the output on an oscilloscope.
Thanks!