Part Number: ADC34J45EVM
Other Parts Discussed in Thread: LMK04828
I am using ADC34j45EVM with FPGA. I follow the steps in the user guide:
1. The evaluation of the ADC32J/34Jxx EVM requires programming the LMK04828 clock source with the
correct PLL settings to provide a 160 Msps clock.
• Connect a USB cable from the ADC32J/34Jxx EVM to the PC
• Open the ADC3000 GUI, and connect to the ADC32Jxx or ADC34Jxx EVM
• Go to the Low Level tab and click Load Config
• Browse and find the ADC3xJxx_160MSPS_Operation_LMK_Setting.cfg
• Check that the PLL2 LED D4 is lit – this indicates that the PLL is programmed properly and the
correct clocks are being generated
After I loaded the "ADC3xJxx_160MSPS_Operation_LMK_Setting.cfg" . The PLL2 LED D4 is lit.
However, I found the clocks GTX_CLKP/M and CLK_AL0_0P/M in circuit schematic have no output. Why? Is there any setting?