Hi,
One customer is asking whether the DAC5670 is available on an EVM which has an FMC connector? He wants to connect it to the ADC12D1800RFRB, which has an FMC connector at its output.
Thanks!
Marjorie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
One customer is asking whether the DAC5670 is available on an EVM which has an FMC connector? He wants to connect it to the ADC12D1800RFRB, which has an FMC connector at its output.
Thanks!
Marjorie
Hi Marjorie,
I recall the DAC5670 EVM has the HSMC connector, and it should be able to connect to FMC connector via our HSMC to FMC adapter board
http://www.ti.com/tool/fmc-dac-adapter
The High Rel team should be able to comment more on this and double check the pin out between the adapter and the EVM. I will let them know about this post.
-KH
Hi,
can I ask you the following questions...
In our project we want to use the DAC5670 in combination with the Virtex4 (ML402) evaluation board.
Of coars it would be perfect if we could buy first an DAC 5670 evaluationboard to test the whole stuff.
But on the internet, I didn't find a DAC5670 evaluation board.
Is there any solution to do this ? Where can we buy all this stuff ? (The virtex4 ML402 we have allready.)
Many thanks in advance.