Dear Sir/Madam
I'm working with the ADC12J4000EVM (the former version, with the LMX2581 Synthesizer) and the TSW14J56 (rev B). I use external clocking to reach 4GSPS and up to there everithing work fine.
I want to use the TimeStamp feature but when I remove R19 and R20 in order to connect the timestamp SMAs, I always got a time out error in HSDC (v4.1). However in the ADC12J4000EVM GUI (v1.3 but in Help\about it says v1.0) enabling the timestamp or not and toggeling the Single-Ended SYNC~ select doesn't help.
NB : I didn't connect anything yet to the Timestamp SMAs since the ADC12J4000 datasheet says that those pins can be left unconnected if unused.
Could you help me to use the single ended SYNC~ pin to provide JESD synchronization in order to release the SYNC~/TMST pins for timestamp function ?
Yours sincerely
Maxime D.