Other Parts Discussed in Thread: ADC12J4000
I read in the user manual that the ADC12J4000 has DIFFERENTIAL INPUT via board modification, just wondering how to perform the mod?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADC12J4000
I read in the user manual that the ADC12J4000 has DIFFERENTIAL INPUT via board modification, just wondering how to perform the mod?
Hi Rajesh,
Here are instruction to go from single-ended to differential input on ADC12J4000
1. S/E input, AC-coupled:
a. Default populate option
b. Balun is {400MHz, 3GHz}
2. Differential DC-coupled:
a. Remove C3, C5.
b. Populate C1 = C6 = 0 ohm.
3. Differential AC-coupled:
a. Remove C3, C5.
b. Populate C1 = C6 = 100 pF.
This information is also available on the first page of schematic for adc12j4000 evm which can be downloaded from TI website(it is under adc12jxx00 design package folder).
I have also attached the snapshot below.
Here is the link

Regards,
Neeraj Gill