Part Number: ADC32RF45
Other Parts Discussed in Thread: LMX2582, LMK04828, LMK04610
Doing an architecture analysis for a proposed receiver with the ADC32RF45. The ADC will be clocked at 3 GSPS, and Decimation mode will be set to divide-by-24 complex. Need to understand the lowest power clocking configuration. The assumption is a LMX2582 will be used to generate the CLKIN signal for the ADC. What is the best low power option to generate SYSREF(s)?
The EVM uses the LMK04828 to generate SYSREF and the FPGA Clock/SYSREF. But this seems like a high power solution for generating SYSREF as the data sheet shows the LMK04828 consuming about 1.9W. This spec assumes all outputs are enabled, so maybe its lower in the described operating scenario where only a few outputs are needed. Or maybe there's an alternate method/device to generate SYSREF?
Speaking of power, how does selection of the decimation mode impact power? Data sheet specifications show power dissipation at 6.5-7W, but in bypass mode. Also, does more decimation help the power consumption of the JESD SERDES block since the output rate rate is lower?