Other Parts Discussed in Thread: CDCE72010
Hi,
I want to use the ADS62P49EVM with the onboard-clocking using the onboard CDCE72010 ("Clock Option 2" as described in section 2.2.4.2 of the User Guide).
For this configuration, I need a chrystal filter of 245.76 MHz, which unfortunately is not populated by default. The desing is obviously meant for a certain filter, as there is onboard matching and a certain footprint, however there is no hint in the documentation for specs of this filter other than the center frequency.
Can anyone give me a hint which filter I can use here?
Alternatively, I could use "Clock Option 3" using the LVPECL connection which does not need this filter. However, section 2.2.4.3 sais this option is "not recommended for SNR critical applications". Why is that so? What is the issue with this configuration? I have seen LVPECL connections between clock cleaners and ADC/DAC devices in many Appnotes, so this seems a quite common way to go.
Thanks for your help,
Stefan