Part Number: TDC7200
Other Parts Discussed in Thread: TDC1000, , TDC7201-ZAX-EVM
Hi,
I've been working on a design which uses TDC1000 and TDC7200.
I've had no issues with using SPI to configure TDC1000, but the TDC7200 has been misbehaving.
The device seems to be quite reluctant in sharing the SPI bus with other devices. Even connecting a Data Analyzer to the SPI bus, renders it non functional.
I've debugged to issue to the MISO line (DOUT for TDC7200). My design uses two TDC1000´s and two TDC7200´s. While the TDC1000´s have no issues coexisting, the moment I connect the 2nd TDC7200, both stop working.
I'm using a 33 Ohm resistor near each DOUT pin.
Why? Workaround? Should I use a Tri-state buffers on each of the TDC7200 MISO lines?
Best Regards,
José Caeiro