1. Is the full scale of this ADC is 4*Vref when it works with two differential input? The scale of input defined in the table 1 and the description in the previous paragraph"Each analog input signal should have a peak-to-peak voltage equal to the input reference voltage, VREF , be centered around V REF and be 180° out of phase with each other." are not accordant.
2. If the input of Vin+ and Vin- are not reach to Vref, the output binary code is centered on 2048?
3.Is the Vcm changeless, and the input on Vin+ and Vin- centered 0V is ok or the circuit should ensure the input on Vin+ and Vin- is centered Vcm?