Hello
I am trying to access JESD bank 0x6800 , 0x6900, 0x6A00. But I am unable to readback from the registers mentioned in these. Device clock of 200 MHz and continuous Sysref of 3.125 MHz is applied and I am giving hardware reset also after power up and digital reset also.
I am able to do write read in Analog Bank
Following are the register access commands
NOTE - adc_jesd_write is write function for spi write and adc_jesd_read is read function for spi read.
adc_jesd_write 0x0000 0x81
adc_jesd_write 0x4001 0x00
adc_jesd_write 0x4002 0x00
adc_jesd_write 0x4003 0x00
adc_jesd_write 0x4004 0x68
adc_jesd_write 0x60F7 0x01
adc_jesd_write 0x6000 0x01
adc_jesd_write 0x6000 0x00
adc_jesd_write 0x0011 0x80
adc_jesd_write 0x0059 0x20
adc_jesd_read 0x0059 ---- THIS WORKS FINE
adc_jesd_write 0x4003 0x00
adc_jesd_write 0x4004 0x69
adc_jesd_write 0x6000 0x80
adc_jesd_read 0x6000 ---- THIS DOESN'T WORK
adc_jesd_read 0x6001 ----- THIS DOESN'T WORK
KIndly help to resolve this issue.
Regards
Shashank