Other Parts Discussed in Thread: LMH5401, LMH5401-SP
Hello,
I'm trying to understand the absolute maximum ratings for the analog inputs of this device.
In Table 6.1 of the datasheet, the abs max for the four Vin pins is given as -0.15v to +2.5v with the note "while maintaining common mode" and the additional note 3 saying that this is verified at VA = VD = 2.2v. Normally I would expect that an absolute maximum rating expressed this way (as an absolute value, 2.5v, not related to supply rail) would be valid at any permissible supply voltage, but note 3 makes me wonder (with a 2.2v supply, we can expect the protection diode will not be conducting much for Vin = 2.5v). That's my first question: is the +2.5v absolute maximum for the four Vin pins valid irrespective of the value of VD or VA?
My second question relates to the -0.15v rating. In Table 6.3, Recommended Operating Conditions, the minimum voltage at the four Vin pins is specified as -0.4v. This seems to violate the abs max rating on the face of it, so I wonder how to reconcile that. That's my second question: Is the -0.15v absolute maximum rating valid? How can the recommended be outside the absolute max?
I am designing a data converter system for a Mars exploration mission, and I'm needing to prove device safety for anomalous conditions, such as during power up or test, when one supply of the driving device may be unpowered. In this case both inputs might be driven above the 1.9v rail or below ground, but there are series resistors which would limit the current to below the +-50mA maximum, assuming the protection diodes turn on. But I don't think it's possible to limit that voltage to -0.15v without some other clamp. And, if the +2.5v rating should really be expressed as VA + 0.3v, the same problem applies to the positive excursion.
Thanks for any help
Rick Raffanti
Techne Instruments, Inc
(contractor for Southwest Research, San Antonio)