Hello
what is the ADC common mode voltage set to on this EVM in the default ac coupled configuration or do I need to supply this? I will have an input signal that swings from 0-1.9V, I take it that this is the limit, are the input transformers 1:1?
what is the range of ADC sampling rates that I can set on this EVM, I would like to test at 100MSPS, 200MSPS, 500MSPS, 1GSPS. Is this possible with supplying a 10MHz external reference to the onboard clocking solution. I would like to synchronize other boards hence the use of the external 10MHz reference.
Thanks