Hi people
Im working on the design of two channel bipotentiostat/galvanostat and im going to use the DAC8871 as a signal generator (voltage ramps basically) because of its capability of working with different dual references (which means different spans of generation)
The thing is... what is the best output filtering i should use with this device? Is it a passive filter or an active filter (my solution would be a 2nd order sallen key with 1kHz) but i dont know how much will this affect the accuracy of the system... or if i should use only an ompamp buffer as suggested on the datasheet (with an opa277)
I have another question about the major carry glitch; if im understanding the datasheet correctly... i will only have the glitch when im using the "enable" LDAC? If im not using it (if i have it tied low), then i dont have to worry about the major carry glitch (i know it will be there... i just want to know if it will be smaller and how much)
Thank you very much for your time and your answers