Is there any reason that the ADS1299 can be powered with a unipolar supply, AVDD = 5V & AVSS = 0 V, or a bipolar supply, AVDD = 2.5V, AVSS = -2.5V?
Why would one pick one method of supplying power over the other? Thanks!
Alex
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any reason that the ADS1299 can be powered with a unipolar supply, AVDD = 5V & AVSS = 0 V, or a bipolar supply, AVDD = 2.5V, AVSS = -2.5V?
Why would one pick one method of supplying power over the other? Thanks!
Alex
Hi Alex,
In terms of performance, there really is no difference.
I think what you need to be concerned with is the acceptable voltage ranges for your input channel pins. With a single-ended supply of 0-5 V, your input pins will not be able to take singles below ground; instead, they will be saturated and the output will read "negative full-scale."
Bipolar supplies avoid this concern and allow each input pin to receive voltages above and below ground.
If you expect your input signals to have a large common-mode, you can use the "patient bias drive" amplifier to adjust the common-mode of your inputs to within the AVDD-AVSS range.
Thanks and regards,
Hi Ryan, please explain how to configure VREFP when we use bipolar power supply+-2.5V.
If VREFN=AVSS=-2.5V then we need to apply +2.5V reference from external source to VREFP?
Or we can configure internally to obtain right non-saturated readings?
Regards
Hi George,
With +/- 2.5 V supplies, you have the option of using either an internal or external 4.5 V reference. The internal reference is 4.5 V +/- 0.2%.
Using the external reference, as you alluded to, would require applying an external voltage to VREFP. Keep in mind the requirement that VREFP = AVSS + 4.5 V. With +/- 2.5 V supplies, VREFN = AVSS = -2.5 V, so you cannot apply more than +2 V on VREFP.
Regards,
Hi Ryan,
Thanks for full answer.
Please answer just last little question for understanding.
If we have VREFN=-2.5V and VREFP=+2V does this mean we have unbalanced inputs?