Other Parts Discussed in Thread: ADS1299
I'm using ADS1299 EVM. I set all jumpers as shown. But i’m not getting a correct signal. Could anyone help to check this setup? Is there anything to be adjusted?
I'm using single-ended inputs. The input electrodes connect to the +pins of CH1 and CH2(pin32&36 of J6).
I'm kind of confused with the reference electrode and bias electrode. I have closed the SRB1 bit in software. Should i remove the jumper on pin1&2 of JP25 and have bias electrode connected to pin2? And where should i have my reference eletrode connected? By connecting pin5&6 of JP25, REF & BIAS are connected together, does it mean i only need a bias electrode?
Another problem is the 50hz-frequency interference. what shoud i do on the board to decrease this interference, or it is supposed to be like this and i have to decrease it by after processing?
THANKS.