Other Parts Discussed in Thread: ADS7830
Hello,
I have got an end product I should repair. There is an analog joystick connected to ADS7830. It is using pins 1 to 3. Each of the inputs is tied down to GND by a 10k resistor.
The problem is that sometimes it has 5V on the input pin3 /same as the supply voltage/, although the joystick is not connected. It is not a problem of wiring or PCB. I've measured the inputs with an oscilloscope and I found that actually there are pulses with timing similar to SDA pin - SDA input is 3.3V because of the MCU. Osciloscope paramters: 1V/div; 2ms/div. Please, see pictures below.
However, sometimes, when the device is restarted it worked fine - there is no voltage on the inputs. So, the question is if it is a chip failure or bad initialization? 
Fig.1 Schematic diagram
Fig.2 Pin3 reading with no input
Fig.3 SDA pin