Hi,
I'm using an ADS1299 to record EEG. However, I would also like to measure the impedance(AC) and the electrodermal activity(EDA) simultaneously from the same electrodes. Is either of them supported by the chip ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Eohan,
Unfortunately the ADS1299 does not have this capability. This post has information about some TI designs to do body impedance and EDA (in the post it's called GSR) using the AFE4300.
Regards,
Brian Pisani
Hi Brian,
Thanks for the feedback. Is it possible to use the DC lead off detection to measure the body impedance between two electrodes? Page 31 on datasheet mentions that ADS1299 could do DC lead off detection simultaneously with EEG capture.