Part Number: ADS1292RECG-FE
Other Parts Discussed in Thread: ADS1292ECG-FE, ADS1292
Hello myself and my counterpart have tried to get the ADS1292-ECG-FE Demo Kit software, ADS1292EVM_SW_v1.11 running on several different machines including both WIN7 and WIN10 Machines. Every time this software has been installed on any of the PC's and the program is executed we get the following Error that pops up upon running the application...when I try to read the registers it shows the progress bar as if it is doing something but no values are shown in the window. The Microsoft C++ package also has been installed on each of these machines. I am well aware that this software has not been vetted on WIN10 but I have tried to run this on 2 different WIN7 machines with the same result as shown below? Any advice?
I would also like to inquire about getting the source for the MSP430 that is on the ADS1292R-ECG-Demo board along with the Graphical/PC software as I have read this source is available upon request.
Regards,
Frank