Other Parts Discussed in Thread: ADS1292, ADS1292R, ADS1298
Hello,
I have based a PCB design from the ADS1292R-FE Eval board schematic. I would like to understand how to go about correctly using RLD in being able to derive an ECG waveform. I get it that RLD can be used to reduce common mode voltage/interference. What I am not fully understanding is how to actually make use of the RLD electrode/signal in deriving say a LEAD 1 (RA-LA) output signal. For LEAD 1 on the ADS1292R-FE Eval from everything I can see if should simply be the output on CH2 of the ADC.
So now my questions...
1) To make use of the RLD to reduce common mode voltages in the readings from the ADC is the idea to measure the RLD voltage on each channel and then subtract this value from the ADC channel output?
2) The explanation of the RLD functionality in the ADS1292 Explains the Mux functionality of the RLD but does not explain how to actually make use of the RLD drive. The description on page 50 of the DS shows RLD signal generated from CH1 and then fed into CH2 Negative? It does not explain why anyone would do this. It would be very useful to have an example shown with the ADS1292R-FE Eval board.
I would really like to know how to make use of the RLD signal to provide better results with the ADS1292R with the assumption the hardware is configured as the ADS1292R-FE Eval board is with electrodes matched to ADC channels in particular ELA & ERA connected to IN2P and IN2N respectively. So how does one effectively make use of the RLD measurement/signal?
3) For the case of the ADS1292R-FE Eval board and in reviewing the MSP430 firmware I could not find anywhere where the RLD signal was used in conjunction with an ADC Channel? Maybe I missed something.
Regards,
Frank