Other Parts Discussed in Thread: DAC7574, DAC6574, DAC8550, OPA188, OPA656, LMP92066
I'm looking to use the TPL0102-100 as an I2C rheostat to control the output voltage setting of a TPS7A3301 regulator. This is tricky because the output voltage is negative. My idea is to shift all the voltages of the TPL0102-100's operating environment down to -6.5V, so that all of the datasheet requirements are shifted to a lower equipotential "GND." Then, I want to use isolated coupling to connect SCL and SDA from my main environment to the TPL0102-100.
Has anyone else tried anything like this for I2C adjustment of a negative-voltage regulator? For the schematic drawing attached, are there any reasons why this concept would NOT work?