The RVS pin on this part is overloaded to provide the internal ADCST as well as to provide the clock in SRC mode transfers. What is the behavior of RVS if we are doing a SRC transfer in Zone2 mode?
RVS will go low in response to CONVST. If we now pull CSn low to do a data transfer (after Td_cnvcap), RVS will start toggling within 40ns per datasheet Fig 6. After the transfer is done, if we pull CSn high, RVS is expected to return high within 70ns per that same timing diagram. However, if the conversion is still in progress, RVS is expected to be low for Tconv_min=300ns (datasheet Fig 43). So in this case, will RVS return high (following CSn deassertion) or stay low (till conversion is done)?
What happens if the data transfer is happening during the Tconv_min to Tconv_max window where RVS is expected to go high? Does the data transfer timing/behavior take precedence over the conversion process timing/behavior for the RVS pin?