Part Number: ADS1258
Other Parts Discussed in Thread: LMV358, OPA320
I am using the ADS1258 in a design that measures a 0 - 5V signal. I have the ADS1258 configured to take a sample every 64 Hz using the pulse convert command.
(note: the voltage divider components on the AIN6 line. These have been removed/shorted for this test.)
I noticed that when the ADC conversion is taking place, the AIN6 line has significantly more noise on it. The noise looks like a ramping signal.
I've taken some screen shots of my oscilloscope to show the issue.
1. ADC_START pin low, measuring 2V signal into AIN6 while the ADC is not converting.
2. ADC_START pin high, measuring 2V signal into AIN6 while the ADC is converting.
3. ADC_START pin low, measuring 4V signal into AIN6 while the ADC is not converting.
4. ADC_START pin high, measuring 4V signal into AIN6 while the ADC is converting.
It seems that as the input signal increases in amplitude the noise/ramping also increases.
Is this noise/saw tooth signal caused by the internal ADC caps charging and discharging while taking samples? Is this considered normal?