Part Number: ADS8568
The documented details of writing to the configuration register in this device are contradictory and confusing.
We are using the device is in Software Mode with the Parallel Interface enabled.
On page 8, the description of REFEN/WR says, "The parallel data input is enabled when CS\ and WR\ are low." OK, makes sense.
On page 19, Figure 3 is Parallel Write Access Timing Diagram, and it shows that CS\ and WR\ start high, and then CS\ and WR\ are brought low while DB[15:0] is driven with the upper configuration word. WR\ is brought high for tWRH and then brought low with the lower configuration word on DB[]. CS\ remains low this whole time. Then WR\ is brought high followed by CS\ going high.
On page 35, Figure 40, we see for Parallel mode that CS\ can remain low for both of the WR\ cycles, or it can go high between them (along with WR\ going high). Not the same as what is stated on page 19 but close.
And finally, the kicker. On page 34, section 9.4.2 Software Mode we read in the second paragraph,
"Do not hold CS low during these two accesses."
And that completely contradicts all of the other statements about the configuration writes.
What is the correct timing/operation for the configuration register write in parallel mode?
And can the data sheet be fixed to correctly show how you're supposed to use this feature?