Hi, when negative charge pump enabled, we can accept as low as AVSS-1.5V input at VINP and VINN.
So when I apply AVDD=3V, VREF=3V, VINN=1.5V, VINP ranges from -1.5V to 1.5V, the ADC can still work well, right?
The only bad effect is that the input is equal to -3 to 0V range, so the corresponding digital output will not be full scale, only 0-2^23, right?