Other Parts Discussed in Thread: ADS1261, ADS1260, REF6025
Hello -- I wanted to confirm that the ADS1271B will function with a VREF+ of 5.0 V VREF- of 0V, AVDD of 5.0 V and DVDD of 1.8/3.3V.
The source of confusion is that under "Electrical Characteristics" on page 4 of the datasheet (http://www.ti.com/lit/ds/symlink/ads1271.pdf
equations on page 17 appear to allow a 5V VREFP. Additionally, the Webench reference selector recommends a 5V source.
Ultimately, I plan to connect the muRata SCA103T inclinometer (https://www.murata.com/~/media/webrenewal/products/sensor/inclinometer/sca103t/sca103t_inclinometer_datasheet__8261700a3_0.ashx?la=en-usan ADC -- so if this ADC doesn't work at a 5V VREF+ voltage, please recommend one that does.
Thanks!
Mark