Hello,
We are working with CC2650F128 to read strain gauges.
So far we have been using the ADS1231 to read a differential input and it worked just fine. Now we want to increase the system's capability to incorporate multiple bridge sensors.
To reduce chip count and pin usage from the MCU we have decided to use a multi-channel ADC instead of adding ADCs to the SPI bus.
The main requirments are:
- Low-power mode.
- High precision.
- SPI compatible.
- At least 3 bridge sensors (8-channels).
- Sample rate < 1 kSPS.
- Supply voltage of 3.3V. COuld go up to 5V if necessary.
We are considering the ADS1148 or it's "next generation" the ADS114s08. (We think that 16-bit is enough for our aplication).
An alternative would be to have multiple ADS1120 (from which we like the power performance) in the SPI bus. This would only be worth doing if the precision and power performance compensate.
But we are still deciding, any suggestion on alternative ADCs would be much appreciated.
Are there any ADC preferred for bridge sensor with multichannel and low-power?
If only there was a low-power equivalent for ADS1262...
Best regards,
Max