I'm running CCSv4 on Windows 7 in a virtual machine with Ubuntu 11.04 as the host. I'm trying to debug a program ment to run on the OMAP L-138, which lives on a custom evaluation board. I keep running into this error every time i go to debug:
Error connecting to the target:
(Error -600 @ 0x0)
A required dynamic library could not be located.
The library isn't on the search path.
(Release 5.0.333.0)
I've got the correct XDS100v2 USB Emulator Installed and am using Version 4.2.3.00004, so Im not sure where the 5.0.333.0 release is coming from -- well maybe I do, I previously had version 5.0.333.0 running on my Ubuntu Host and Version 4.2.3.00004 running on a Windows virtual machine. I've since uninstalled version 5 and still keep getting this error. If i had a little more information on what Error -600 was, i might be able to fix the missing library it speaks up. Any insight as to the cause of this error?
Thanks,
Christine