What is the difference between "Spectrum Digital XDS510USB-PLUS Emulator via JSC" and "Spectrum Digital XDS510USB Emulator" in the CCS Target configuration ?
I am using the XDS510PLUS with TMC320C6678 , I am using the 14-pin JTAG interface.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the difference between "Spectrum Digital XDS510USB-PLUS Emulator via JSC" and "Spectrum Digital XDS510USB Emulator" in the CCS Target configuration ?
I am using the XDS510PLUS with TMC320C6678 , I am using the 14-pin JTAG interface.
Hello,
There is a description in the readme from Spectrum Digital:
"Supports limited use of the XDS510USB-PLUS emulator via the TI JSC interface. This allows TI XDS510 class emulation drivers to run with the XDS510USB-PLUS in same manner as XDS100v2. The performance in this configuration is roughly the same as the XDS100v2. This is not supported on the XDS510USB as the USB 1.1 full speed port in combination with TI JSC is to slow to be useful"
Hope this helps,
ki