This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccsv5.1.0.0800 does not allow breakpoint in linked file

Guru 15580 points


FYI. The M8 build is having trouble with breakpoints set in linked files. It also has trouble with ctl+R (run to line). This did not occur in M7.

Thx,

MikeH

 

  • Ugh, that is a nasty one. I just tried this out too on M8 and I see the same issue. On M8, the breakpoint manager seems to be pre-pending the compilation path to linked file path for the full path to the file, thus creating an invalid path to the source file. Strange.

    I filed a bug. The ID is: SDSCM00041826

    Thanks

    ki