CCS seems to automatically collapse all expanded expressions in the watch window when you return from a function call. Irritating....:(
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mike,
There is unfortunately, as thought, no way to change this behaviour.
I have filed this in our system as a potential enhancement. This is the number and the link contains the information you need to track it if you wish.
SDSCM00041843
http://processors.wiki.ti.com/index.php/Compiler_Defects_Database
I hope this clarification helps.
Best Regards,
Lisa
Lisa,
Lisa TI said:no way to change this behaviour.
That *is* unfortunate. This is a serious problem for serious debugging. I could understand it the expression was "local" and you exited the context of the expression that i would close. But these are globals. They should remain open all sections of code.
When do you think this might get incorporated?
Thx,
MikeH
Hi Mike,
I can not say or make any guaratees. I have submitted it as a potential enhancement and hopefully it will be something that comes and quickly.
You can follow the submission using the number and link I put in my previous post. You will be able to see the status updates etc.
Best Regards,
Lisa
Hello,
It has been almost 4.5 years since the last post in this thread. Is this issue going to be fixed in the next revision? I would consider this issue more towards the major side than minor. It doesn't exactly stop me from doing my work, but it does slow me down considerably.
Stephen