This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with Code Composer 4

Other Parts Discussed in Thread: TMS320C5535

I bought the TMS320C5535 eZdsp board and installed Code Composer 4 as instructed in the QuickStart guide.

When folowing the guide to set up the CCS configuration and get to the step to connect the target, I get

the following error:

Error connecting to the target:
(Error -600 @ 0x0)
A required dynamic library could not be located.
The library isn't on the search path.
(Release 5.0.429.0)

Where is this library and how do I get it in the search path?

I also notice that in the Windows7 device manager that there is no driver installed for TMSC5505.

Shouldn't the driver have been installed during the CC4 software install?