Other Parts Discussed in Thread: TMS320F2808
One of our developers is getting an error during build: "This project was created for a device-variant that is not currently recognized: TMS320C28XX.TMS320F2808. Please install the device-variant descriptor, or migrate the project to one of the supported device-variants."
This is odd because we store projects on SVN. It builds fine on two other development boxes, but when he pulls the files, including the .cdtproject, .ccsproject, and .cdtbuild, he gets an error. This has worked fine in the past. He's tried to build versions of the software that he could previously build with the same result.
From the other posts with this error, we've tried restarting, clearing the workspace and re-importing the project, and we've verified that the .cdtbuild file is the same as what compiles on the other boxes. (We've also pulled the files from SVN again, just to be sure)
We're on 4.2.3.00004, and we cannot upgrade.