Hi,
I am running some test code on C6748 (using a OMAP-L138 eval board from Logic PD. I am using the DSP module only and not the module with ARM + C6748).
The board is hooked up to the host machine through a XDSv2 USB emulator and the 14-pin TI connector.
I need to profile the code to understand bottlenecks better. But, when I click on "Profile -> Setup", I do not get options to enable different profiling options.
Is there a way to profile code running on C6748 using CCStudio v5?
Thanks,
-raja.