Hi,
It's the first time I use the graph option in CCS so I'm sorry if I ask something very obvious, but I just can't understand.
I needed to watch the fluctuation of a variable on a graph, so i added the variable in the watch expression window, right clicked on it, clicked graph and the graph appeared.
The problem is it had a sample rate of 1 Hz that's just too low for me, I needed 500-1000 Hz . So I went on Tools->Graph->Single Time and modified the sample rate, then clicked ok. Then, another graph appeared that just didn't made sense to me and if I do again the right click on variable-> Graph selection, the graph has again a sample rate of 1 Hz.
Can you please tell me how I can make a graph of the variable with the sample rate I want (or just obtain the data on a .csv file)?
Thank you